2013-06-04 6:10 AM
Hello I have a strange behaviour with usart (1 and 4) on STM32F217.
I use it as output log. When I build and debug, nothing leaves the STM. After a ''debug'' reset in atollic(a restart) it works fine.I tried these two operations:-after one loop of program, try a soft reset. But not good.-an external reset. But not good.I don't know where to search. I compared register when it works and when it doesn't but no difference (for USART and NVIC).It is exactly the same with DMA and USART transmit. It is fine at the second time (only after debugger reset).If somebody has an idea?Pierre2013-06-04 6:20 AM
Pay attention to whether the HSE and PLL start properly.
Pay attention to the order in which you enable clocks, and start peripherals, etc. Check to see if the code gets stuck in a loop somewhere. Use LED/GPIO to track progress through startup code and initialization so you can pin point where things are failing or stuck.2013-06-04 7:31 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.