2024-09-10 7:35 AM
Good evening community members,
today I have been trying to activate USART module of my STM32F446 board. However even after trying everything, I could not sense Tx signal on PA2 pin of the board. This is the low level code I used. I had been trying to capture the signal using Oscilloscope but got nothing. Could someone help me how to resolve the issue? I tried my best but found nothing so far. Thanks in advance.
#include "stm32f4xx.h"
#include <stdint.h>
#include <stdio.h>
void gpio_init(void)
{
RCC->APB1ENR |= (1U<<17); //enable clock for USART2
GPIOA->MODER |= (0b10<<4); //setting PA2 in alternate function mode
GPIOA->AFR[0] |= (0b0111<<8); //setting PA2 in AF7 mode
RCC->AHB1ENR |= (1U<<0); //enable GPIO Port A
}
void usart_init(void)
{
USART2->BRR = (0x8B); //setting baud rate as 115200
USART2->CR1 = (1U<<3); //transmitter enable
USART2->CR1 |= (1U<<13); //enable USART
}
void usart2_data(char c)
{
while (!(USART2->SR & (1U<<7))){}
USART2->DR = c;
}
#include <usart_tx.h>
int main(void)
{
gpio_init();
usart_init();
while (1)
{
usart2_data('Y');
}
}
2024-09-10 8:13 AM - edited 2024-09-10 8:40 AM
Hello @Yoshimitsu_Manji_clan,
Ensure that UART settings (stop bits, word length, parity, baud rate...) are configured correctly.
Check if there is no other peripherals are interfering with PA2.
2024-09-10 8:23 AM
Recheck your baud rate calculation.
2024-09-10 10:28 PM
Baudrate calculations are as follows:
USARTDIV = (16 * 1000000)/(115200 * 16) = 8.68
Mantissa = 8
Fraction = 0.68 * 16 = 10.88 ~~ 11
Hence BRR = 0x8B
2024-09-10 11:49 PM
GPIOA->MODER |= (0b10<<4); //setting PA2 in alternate function mode GPIOA->AFR[0] |= (0b0111<<8); //setting PA2 in AF7 mode RCC->AHB1ENR |= (1U<<0); //enable GPIO Port A
You have to set RCC_AHB1ENR.GPIOAEN *before* accessing the GPIOA registers.
You may also want to do that so that there is a delay between setting the clock enable in RCC and first accessing the given peripheral; see errata.
At any case, when in doubts, start debugging with reading out and checking content of the relevant registers.
JW
2024-09-11 12:31 AM - edited 2024-09-11 1:48 PM
The proper formula for BRR is
USART2->BRR = (USART_CLK_FREQ + BAUD_RATE / 2) / BAUD_RATE;
which yields the value of 139 decimal - the same as in you code by a wild chance.
Also, UART CR1 register should be set to:
USART2->CR1 = USART_CR1_TE | USART_CR1_UE;
- it will not work with TE bit clear.
The main problem with you code is what @waclawek.jan wrote - GPIOA not enabled during config.
2024-09-11 11:00 PM
In my code I have set TE bit as 1
USART2->CR1 = (1U<<3); //transmitter enableAlso I have enabled GPIOA before configuring its Alternate Function.
RCC->APB1ENR |= (1U<<17); //enable clock for USART2
RCC->AHB1ENR |= (1U<<0); //enable GPIO Port A
GPIOA->MODER |= (0b10<<4); //setting PA2 in alternate function mode
GPIOA->AFR[0] |= (0b0111<<8); //setting PA2 in AF7 modestill I can't see data pulses at PA2 pin. This pin is not configured for any other purpose in this program.
Anything else I need to check to make it work?
2024-09-12 12:54 AM
Read out and check/post content of UART and relevant GPIO registers.
Make sure the hardware is OK by setting PA2 to GPIO Out and toggling it either manually in debugger, or in program using a simple loopdelay (as in the basic blinky).
JW
2024-09-13 1:35 PM
I meant UE bit, as shown in my code fragment above.
Your code would be a lot easier to read and debug if you used standard bit names instead of cryptic magic expressions.
2024-09-14 2:22 AM
I took the above code with the correction for GPIO clock enable, commenting out #include <usart_tx.h> which I don't have, and in a DiscoF4 it works as expected, transmitting infinitely on PA2, as observed by oscilloscope.
Now if you observe this using a UART receiver (e.g. UART-USB converter, fed into a PC), depending on how it is started, it may get confused by the infinite stream with no spaces if it does not get synchronized properly on the first character. Try to place delays between the characters.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.