2026-03-29 4:04 AM
When a USART is configured without a clock, the code generator treats it as a UART and assigns HAL_UART_IRQHandler as the interrupt handler. However, within this handler, there is a blocking operation during the idle process:(void)HAL_DMA_Abort(huart->hdmarx);
When certain error conditions occur, the code can become stuck in HAL_GetTick(). This happens because the SysTick priority is lower than that of the UART interrupt. I have observed this behavior multiple times, particularly when noise is present on the UART signal line.
Has Anyone seen this situation before?
Solved! Go to Solution.
2026-03-29 7:01 AM
HAL assumes SysTick (or whatever is being used to drive HAL_GetTick) has a higher priority than functions it is called from. It's up to you to ensure this is the case.
2026-03-29 7:01 AM
HAL assumes SysTick (or whatever is being used to drive HAL_GetTick) has a higher priority than functions it is called from. It's up to you to ensure this is the case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.