2018-08-03 5:05 AM
For a 21-channel temperature measurement tool (NTCs) I use a STM32F373 ( SDADC1 + SDADC2 + SDADC3). I replaced a temperature sensor with a fixed resistor for these tests.
The behavior of the ADCs is different and reproducible after startup:
Good Case: The measured values are absolutely stable and correspond to the setpoint
Bad Case: The measured values are not stable and shift with a time constant of approx. 80 seconds. The behaviour of all 3 SDADCs are the same.
The SDADC is configured as follows:
- VREF 2.5V external (stable)
- Continuous Mode
- Single-ended zero-volt reference mode
- gain 1
- Injected conversion
- 9 channels
- DMA mode
Clock configuration:
- 12MHz oscillator on HSE
- PLL on, PLLMul 4
- SDADC Prescaler 32
The following has been tested without success:
- Single-ended offset mode
- Delays after power up
- Sysclk = HSE
- SDADC Prescaler Settings
Thanks Paul
2018-08-03 5:47 AM
So when do you observe the "good case" and when the "bad case"?
2018-08-05 11:48 PM
Hi Jan,
After starting up, the SDADC either works stable "good case" or with a drift "bad case". This behavior is maintained throughout the operating period. The chance that the SDADC works correctly is fifty-fifty. I suspect that the SDADC has a timing problem.
2018-08-06 1:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.