2023-07-11 6:30 AM
For some reason HAL_SPI_STATE remains busy forever after executing HAL_SPI_Receive_DMA. This happen for the SPI slave of SPI #2 of the STM32H745XI board.
The problem goes away when I change the SPI mode from slave to master, but that's not a proper workaround. I want to have a half-duplex communication between a master and a slave SPI. So I need a slave that can receive data via DMA!
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_FMC_Init();
MX_LTDC_Init();
MX_CRC_Init();
MX_DMA2D_Init();
MX_SPI2_Init();
MX_SPI4_Init();
MX_QUADSPI_Init();
MX_TouchGFX_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_TouchGFX_Process();
/* USER CODE BEGIN 3 */
HAL_SPI_Receive_DMA(&hspi2, RX_Buffer, sizeof(RX_Buffer));
while(HAL_SPI_GetState(&hspi2)!= HAL_SPI_STATE_READY){} //Gets stuck here forever!!!!
transfer_complete=0;
HAL_SPI_Transmit_DMA(&hspi4, TX_Buffer, sizeof(TX_Buffer));
while(HAL_SPI_GetState(&hspi4)!= HAL_SPI_STATE_READY){}
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_SET);
}static void MX_SPI2_Init(void)
{
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_1LINE;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.FirstBit = SPI_FIRSTBIT_LSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 0x0;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi2.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi2.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_SPI4_Init(void)
{
/* SPI4 parameter configuration*/
hspi4.Instance = SPI4;
hspi4.Init.Mode = SPI_MODE_MASTER;
hspi4.Init.Direction = SPI_DIRECTION_1LINE;
hspi4.Init.DataSize = SPI_DATASIZE_8BIT;
hspi4.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi4.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi4.Init.NSS = SPI_NSS_SOFT;
hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi4.Init.FirstBit = SPI_FIRSTBIT_LSB;
hspi4.Init.TIMode = SPI_TIMODE_DISABLE;
hspi4.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi4.Init.CRCPolynomial = 0x0;
hspi4.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi4.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi4.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi4.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi4.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi4.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi4.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi4.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi4.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi4.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi4) != HAL_OK)
{
Error_Handler();
}
}I even changed the clock speed for the slave and it still didn't solve the problem. HAL_SPI_Receive (polling mode) works fine. I even changed DMA Stream and that didn't work neither.
Could someone with knowledge on SPI/DMA shed some light on this issue?
Solved! Go to Solution.
2023-07-11 11:52 PM
Problem solved!
The slave SPI remains in HAL_Busy_RX state because it's waiting to receive a buffer of size mentioned by the user, which in this case is sizeof(RX_Buffer). It is important to note that SPI slave will remain in busy state even if it receives a buffer smaller than sizeof(RX_Buffer). To solve this problem change sizeof(RX_Buffer) to sizeof(TX_Buffer). Moreover remove the line of code
while(HAL_SPI_GetState(&hspi2)!= HAL_SPI_STATE_READY){}Because the processor needs to execute HAL_SPI_Transmit_DMA for the master to send data for the slave to receive.
2023-07-11 6:31 AM
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(hspi->Instance==SPI2)
{
/* USER CODE BEGIN SPI2_MspInit 0 */
/* USER CODE END SPI2_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI2;
PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_SPI2_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOI_CLK_ENABLE();
/**SPI2 GPIO Configuration
PB4 (NJTRST) ------> SPI2_NSS
PD3 ------> SPI2_SCK
PI2 ------> SPI2_MISO
*/
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
/* SPI2 DMA Init */
/* SPI2_RX Init */
hdma_spi2_rx.Instance = DMA2_Stream1;
hdma_spi2_rx.Init.Request = DMA_REQUEST_SPI2_RX;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_NORMAL;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi2_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi2_rx);
/* SPI2_TX Init */
hdma_spi2_tx.Instance = DMA2_Stream0;
hdma_spi2_tx.Init.Request = DMA_REQUEST_SPI2_TX;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_NORMAL;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi2_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmatx,hdma_spi2_tx);
/* SPI2 interrupt Init */
HAL_NVIC_SetPriority(SPI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI2_IRQn);
/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}
else if(hspi->Instance==SPI4)
{
/* USER CODE BEGIN SPI4_MspInit 0 */
/* USER CODE END SPI4_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI4;
PeriphClkInitStruct.Spi45ClockSelection = RCC_SPI45CLKSOURCE_D2PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_SPI4_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/**SPI4 GPIO Configuration
PE2 ------> SPI4_SCK
PE4 ------> SPI4_NSS
PE6 ------> SPI4_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_4|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI4;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* SPI4 DMA Init */
/* SPI4_TX Init */
hdma_spi4_tx.Instance = DMA1_Stream1;
hdma_spi4_tx.Init.Request = DMA_REQUEST_SPI4_TX;
hdma_spi4_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi4_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi4_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi4_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi4_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi4_tx.Init.Mode = DMA_NORMAL;
hdma_spi4_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi4_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi4_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmatx,hdma_spi4_tx);
/* SPI4_RX Init */
hdma_spi4_rx.Instance = DMA1_Stream0;
hdma_spi4_rx.Init.Request = DMA_REQUEST_SPI4_RX;
hdma_spi4_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi4_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi4_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi4_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi4_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi4_rx.Init.Mode = DMA_NORMAL;
hdma_spi4_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi4_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi4_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi4_rx);
/* SPI4 interrupt Init */
HAL_NVIC_SetPriority(SPI4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI4_IRQn);
/* USER CODE BEGIN SPI4_MspInit 1 */
/* USER CODE END SPI4_MspInit 1 */
}
}
2023-07-11 11:52 PM
Problem solved!
The slave SPI remains in HAL_Busy_RX state because it's waiting to receive a buffer of size mentioned by the user, which in this case is sizeof(RX_Buffer). It is important to note that SPI slave will remain in busy state even if it receives a buffer smaller than sizeof(RX_Buffer). To solve this problem change sizeof(RX_Buffer) to sizeof(TX_Buffer). Moreover remove the line of code
while(HAL_SPI_GetState(&hspi2)!= HAL_SPI_STATE_READY){}Because the processor needs to execute HAL_SPI_Transmit_DMA for the master to send data for the slave to receive.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.