2022-02-16 9:52 AM
2022-02-16 9:57 AM
Hi,
I am trying to interface STM32L476RG with NORDIC BLE chip..
My UART 4 and UART 5 individually working fine..
My code inside the while loop is as follows
HAL_UART_Receive(&huart4,(uint8_t*)MSG4,sizeof(MSG4),1000);
HAL_Delay(1000);
HAL_UART_Transmit(&huart5,(uint8_t*)MSG4,sizeof(MSG4),1000);
HAL_Delay(1000);
I want whatever received through BLE ->UART ->STM to come out as is
but I am not getting anything..UART 4 is receiving fine as we were able to check the output
but I am not able to receive and print the same in UART 5..can I know why this is happening??
Thanks and regards
Ravi
2022-02-17 9:35 AM
HI all,
Kindly give me some direction on how to proceed from here...we are stuck..Thanks
Ravi
2022-02-17 12:25 PM
2022-02-18 1:15 AM
Hi piranha,
we are currently not using any DMA in our UART transmission..just a simple messages sequence which we can send from STM to Nordic BLE .
attached is the C code which I am trying..let me know if we need any changes here..if we need to add any driver file.
when I test as individual STM board this works fine..only when integrated to Nordic I find this issue...
when Tx is done(HAL_TRANSMIT) I get ifconfig___end at the other end instead of intended characters..do not know the reason
same when Rx is done(HAL_RECEIVE ) I cannot see any characters received...but till the pins when connected to USB-> UART terminal we are seeing from Nordic..but not inside STM...can we know why this is happening.
Thanks and regards
Ravi
2022-02-21 1:45 AM
Hi piranha,
Any update on my previous query on UART RX and Tx which we are trying to do with NORDIC and STM32..kindly let me know.
Thanks
Ravi
2022-02-21 1:54 AM
2022-02-21 9:46 PM
Hi,
Any update let me know ..we are stuck at this point kindly help us to understand how to procced from here
regards
Ravi
2022-02-21 9:50 PM
Hi,
should I use HAL_UART_RECEIVE_IT for this??..there are no INTERRUPT pin as such ..but still do we need to use this..let me know.
thanks
Ravi
2022-02-22 11:00 PM
HI,
Any update on how HAL_UART_RECEIVE need to be addressed ..Kindly help us through this.
regards
Ravi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.