STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FLASH data is not held

hey thereI have a STM32f030k6t6 which I wish to store data in its FLASH eeprom.the thing is sometimes data on certain addresses are cleared in startup! here is my codeHAL_FLASH_Unlock(); EE_Init();//eeprom initiallization EE_ReadVariable(ID_FLASH_ADD...

Ala by Senior
  • 795 Views
  • 1 replies
  • 0 kudos

STM32F051R8 (64-pin on MB1034B) and RM0091 - can't find alternate function (AF) specifications for PF6/PF7 to enable I2C2.

I'm setting out to configure I2C2 on STM32F051R8. RM0091 (dm00031936) table 13 (pin definitions) has two rows describing pin 47/48 (LQFP64 package) PF6 and PF7 as being configurable for I2C2_SCL and I2C2_SDA.I'm now looking for alternate function (AF...

0693W00000Ka9OiQAJ.png
wb0gaz by Senior
  • 2262 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L476RG VREF 2.5V to AD?

VREFBUF_TypeDef adRef; adRef.CSR |= VREFBUF_CSR_ENVR | VREFBUF_CSR_VRS; adRef.CSR &= ~VREFBUF_CSR_HIZ;Can someone tell me why I cannot set the AD VREF+ to 2.5V?

0693W00000Ka9K7QAJ.png
SWenn.1 by Senior III
  • 1573 Views
  • 2 replies
  • 0 kudos

Resolved! Trigger ADC1 conversion using TIM3 using registers

Hello,I am trying to have analog voltage converted every 2 seconds using the TRGO signal from TIM3. Without much success. For now, I managed to generate interrupt of TIM3 and in TIM3 Handler to use software trigger for ADC. Here is the code:TIM3:void...

UMilo.1 by Associate III
  • 2559 Views
  • 9 replies
  • 0 kudos

[SOLVED] Issue with custom External Loader for IS25LP256D on STM32F746 - update to V2.5.0 & deinit qspi in Init()

I've made a custom external loader for IS25LP256D on STM32F746. It works well in general except for one problem. Verify doesn't stop when "Verify Programming" is checked. Memory-mapped mode works well, which means reading is good. Erase() and Write()...

External loader for external SDRAM

HelloI want to download my code in the external SDRAM connected to a STM32H743 for debugging purpose. I use the STM32CubeIDE, I wrote an external loader .stldr to configure the FMC.In the debugger tab, I selected the external Loader but it fails to l...

GLeco.1 by Associate
  • 1331 Views
  • 1 replies
  • 0 kudos

STM32G option bytes modification fails in DFU mode

I'm working with a host PC running a C++ Visual Studio project which is running some API calls to implement the DFU protocol. Those API are exposed by some DLL and LIB file available with STM32CubeProgrammer. The host PC is connected via a USB cable...

FValm.1 by Associate III
  • 2297 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.