2017-05-05 1:13 AM
In ethernetif driver ethernetif.c in func low_level_input: HAL_ETH_GetReceivedFrame_IT(&EthHandle) can return HAL_BUSY, if ETH_HandleTypeDef state HAL_ETH_STATE_BUSY, if lwIP task is sending data to ethrnet by func low_level_output in this moment. Then func low_level_input willn't run and ethrnet interface will stuck.
Ethernet interface and
ETH_HandleTypeDef struct must be guarded by Mutex.
Can you include this fix to Cube example update?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.