2016-02-21 7:00 AM
Problem is actual in STM32CubeMX (Version 4.13.0 SMT32Cube V1.0) with toolchain IAR EW ARM. When trying to generate code with FreeRTOS with timebase source tuned to TIM3 (or other timer) resulting project has ''HAL_TIM_PeriodElapsedCallback()'' function embedded in ''stm32l1xx_hal_timebase_TIM.c'' module. This module and fuction in it does not contains user code sections, and user can not implement handling of their own interrupts for other timers. Is there any workaround for this problem?
#!timebase #!stm32 #!cubemx2016-02-21 7:19 AM
In addition HAL_TIM_PeriodElapsedCallback() function implemented in stm32l1xx_hal_timebase_TIM.c is
/**
* @brief Period elapsed callback in non blocking mode * @note This function is called when TIM3 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable ''uwTick'' used as application time base. * @param htim : TIM handle * @retval None */void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{ HAL_IncTick();}and have no checking of Callback source, thus any other timer interrupt (if enabled) can lead to the call of this function. It is more correct to use if-condition, like belowvoid HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{ if(htim->Instance == TIM3) HAL_IncTick();}2016-02-21 9:54 AM
I'd go with your latter example where you quantify the source.
2017-05-05 1:01 AM
Hi,
Sorry for the late reply.
This issue was fixed in CubeMX4.15.
We advise you to upgrade with the latest CubeMX release if not already done!
BR. Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.