2020-05-14 9:16 PM
I am currently designing a program using ST32G070 chip.
As a question, I would like to create a program that will change what I was using as a PWM without using Cube Mx into a digital signal LOW or HIGH signal.
I'd like to know how to change it.
2020-05-15 12:42 AM
So you have a pin on which you have a PWM output from a timer, and you want to stop the PWM and set the pin to low or high?
The simplest way is to change the respective GPIO_MODER setting from AF to Out, and then by setting the respective but in GPIO_ODR (through GPIO_BSRR) you set it to low or high. Read the GPIO chapter in Reference Manual.
jW
2020-05-16 8:13 AM
Or if you want to use HAL:
2024-06-08 1:34 PM
Hello,
I have started PWMs
/* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start(&PWM_TIMER, PWM_CHANNEL_U);
HAL_TIM_PWM_Start(&PWM_TIMER, PWM_CHANNEL_V);
HAL_TIM_PWM_Start(&PWM_TIMER, PWM_CHANNEL_W);
HAL_TIMEx_PWMN_Start(&PWM_TIMER, PWM_CHANNEL_U);
HAL_TIMEx_PWMN_Start(&PWM_TIMER, PWM_CHANNEL_V);
HAL_TIMEx_PWMN_Start(&PWM_TIMER, PWM_CHANNEL_W);
/* USER CODE END 2 */
Then configured GPIOs after while loop section which is default place where CubeMX generates.
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
/*Configure GPIO pin Output Level */
/*Configure GPIO pins : PWM_CHANNEL_U|PWM_CHANNEL_V|PWM_CHANNEL_W | GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 */
GPIO_InitStruct.Pin = PWM_CHANNEL_U|PWM_CHANNEL_V|PWM_CHANNEL_W;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
Then, i have stopped PWM's one channel and used that channel as a gpio pin.
/* USER CODE BEGIN 4 */
__HAL_TIM_SET_COMPARE(&PWM_TIMER, PWM_CHANNEL_U, 26);
__HAL_TIM_SET_COMPARE(&PWM_TIMER, PWM_CHANNEL_V, 24);
HAL_TIM_PWM_Stop(&htim1, PWM_CHANNEL_W);
HAL_TIMEx_PWMN_Stop(&htim1, PWM_CHANNEL_W);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_15, GPIO_PIN_RESET);
/* USER CODE END 4 */
But, my code didn't work properly. Any idea about what i am missing?
Thanks a lot....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.