2011-07-19 8:47 AM
Hi,
I am trying to produce PWM signal by using TIM17 channel1 on PORTB-9, but i can't get the PWM signal. In debug mode i can see that TIM17 COUNTER register advanced and do overloop, but i just cant see the PWM signal on PORTB-9. I configured RCC, GPIO and TIM (in this order as seen below). Can any one give a hand? THanks! /************************************RCC*************************************************** /* Setup the microcontroller system. Initialize the Embedded Flash Interface, initialize the PLL and update the SystemFrequency variable. */ SystemInit(); /*Configures the AHB clock (HCLK).*/ RCC_HCLKConfig(RCC_SYSCLK_Div2); /*Configures the Low Speed APB clock (PCLK1).*/ RCC_PCLK1Config(RCC_HCLK_Div1); /* Enable DMA1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* Enable ADC1-Periph, and ADC-GPIO (as defined in MW_hw.h) clocks */ RCC_APB2PeriphClockCmd( RCC_APB2Periph_TIM17 | RCC_APB2Periph_GPIOB , ENABLE ); /************************************GPIO***************************************************GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_Init(MW_CONTROL_GPIO, &GPIO_InitStructure); /************************************TIM17************************************************** /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 11999; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit(TIM17, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse =11999*20/100; //20% TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1PreloadConfig(TIM17, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM17, ENABLE); TIM_Cmd(TIM17, ENABLE); // Enable PWM signal. TIM_CCxCmd(TIM17, TIM_Channel_1, TIM_CCx_Enable); #tim17 #tim-15-16-17-pwm2011-07-20 4:15 AM
Hi,
I have overcome that problem and now it works. What was the problem? TIM15-16-17 are Timer group with complementary outputs and programmable dead-time, therefore PWM configuration is a bit different than TIM2-3-4-5. It mainly require 'BDTR' register configuration. I have attached a working code example for your convenience. Udi.2015-05-27 11:21 PM
I have the same problem. Could anyone post an example code?
Thanks,2015-05-28 7:09 AM
Make sure you initialize all the fields in the time base and output compare structures.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.