2015-05-27 2:22 PM
As you can see here:
https://drive.google.com/file/d/0B979a_DgADKmNkE4N1B0R21BaXM/view?usp=sharing
I'm trying to send data out USART2; it seems to be set up correctly and outputting to pin A14, but the voltage levels don't make sense. It's marking high at 3.3v like it should, but low (space) is over 2v, nowhere near 0. Am I doing something wrong?Must be some setting of the chip, because when I do a hard power-down reset, the problem goes away. Maybe some piece of code on the discovery board is setting something.2015-05-27 3:43 PM
The PA14 pin is the debug interface's clock pin, it's driven by the DISCO's ST-LINK chip.
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00118944.pdf
2015-05-28 8:46 AM
Ah, thanks. Then won't be a problem in production. Looks like A2/A3 are used by the touch sensor, so similar issue there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.