2017-05-15 1:43 AM
Hello dear forum,
I am using F103RC to drive 2 DC motors
Thats why I need to use both TIM1 and TIM8
However TIM1_CH2 is at the same pin as the USART1_TX
I dont use and init USART1_TX pin becouse I only use RX input of USART1 during runtime
I initialize serial port 1 before TIMers
However I noticed that TIM1_CH2 doesnot produce PWM signal and is always at 2.6 V level
I suspect that USART1 is preventing TIM1_CH2 from producing PWM becouse
when I dont init USART1 there is PWM signal
Am I right ? why is that so ?
Can I not only use RX pin (A10) for USART while using A9 port for PWM ?
Thank you
#stm32f103-usart-tim2017-05-15 2:13 AM
Remap in F1 can only remap all GPIO of some peripheral. There is no way whatto achieve what you want to achieve with the pin setup you have. Play around with graphical Cube pin allocation and/or read rm0008, Cha 9.3.7 and 9.3.8 to see if you can find a combination that works for you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.