2017-03-20 5:57 AM
Hi all,
I am not able to get SPI working on stm32l151rbt6a. I have posted my initialization code below.
/* SPI1 init function */
void MX_SPI1_Init(void){ GPIO_InitTypeDef GPIO_InitStruct; SPI_HandleTypeDef hspi1;__SPI1_CLK_ENABLE(); // clock ok
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK PA6 ------> SPI1_MISO PA7 ------> SPI1_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_VERY_LOW; GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLED; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; HAL_SPI_Init(&hspi1); __HAL_SPI_ENABLE(&hspi1); }I am writing a byte to DR and waiting for RXNE bit to set. RXNE bit is never setting. What could be the problem? I have spent a lot of time trying various options but to no avail. Any help will be highly appreciated. Thank you in advance.
2017-03-21 7:38 AM
Hi
Nayani.Parmin
,I'd highly recommend you to refer to the SPI examples under
package. The 'SPI' examples are found under the path below:STM32Cube_FW_L1_V1.6.0\Projects\STM32L152RE-Nucleo\Examples\SPI
Those examples runs on STM32L1xx devices; They will help you to correctly configure the SPI peripheral.Khouloud.
2017-03-21 9:16 PM
Hi Khouloud,
As a matter of fact I used the code generated by Cube only. However I will go through the link, check and revert. If you have worked on this controller SPI, did you get it working? Thank you.
2017-03-22 5:04 AM
Hi
Nayani.Parmin
,The examples are working conveniently.
Khouloud.
2017-04-06 1:02 PM
are you able resolve the issue.. ? if yes, can you please let me know the solution, i am encountering the same issue at my end.
2017-05-15 4:14 AM
Hi Sampath
Sorry I saw your post so very late. I have been able to get SPI working on STM32L151 controller. Let me know if you still have the problem. I will post the code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.