2019-02-10 7:27 PM
Hello,
I am using timer as stm32f401.
However, the clock set in CubeMx is different from the actual clock. (I set it to 48Mhz, but I get 2Mhz when measuring with an oscilloscope.)
I used the MCO pin to measure the PLLCLK clock, but my set clock does not come out.
Where should I look for a solution?
Solved! Go to Solution.
2019-02-10 8:23 PM
Perhaps by looking at the code in SystemClock_Config(), and printing out the speeds
printf("Core=%d, %d MHz\n", SystemCoreClock, SystemCoreClock / 1000000);
printf("HCLK=%d\n", HAL_RCC_GetHCLKFreq());
printf("APB1=%d\n", HAL_RCC_GetPCLK1Freq());
printf("APB2=%d\n", HAL_RCC_GetPCLK2Freq());
Look at the TIM2 setup code.
Check your input clock if using HSE
2019-02-10 8:23 PM
Perhaps by looking at the code in SystemClock_Config(), and printing out the speeds
printf("Core=%d, %d MHz\n", SystemCoreClock, SystemCoreClock / 1000000);
printf("HCLK=%d\n", HAL_RCC_GetHCLKFreq());
printf("APB1=%d\n", HAL_RCC_GetPCLK1Freq());
printf("APB2=%d\n", HAL_RCC_GetPCLK2Freq());
Look at the TIM2 setup code.
Check your input clock if using HSE
2019-02-10 9:05 PM
I checked as you told me.
The settings are out of order. However, checking the SystemClock_Config () created by cubemx did not find any problems.
The output of the compiler is shown below.
Core = 16000000, 16 MHz
HCLK = 16000000
APB1 = 1000000
APB2 = 1000000
Below is the configuration code generated by CubeMx.
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 96;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
Please let me know if there are any misconfigurations (HSE clock is good).
2019-02-10 9:19 PM
You should use the debugger, break point the SystemClock_Config() and check that it is actually being called.
2019-02-10 9:40 PM
Debugging at the start and end breakpoints of SystemClock_Config (). It seems to work correctly by entering a function.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.