2018-05-03 7:44 AM
I have developed dozens of products using the STM32 Family, but can not find an easy solution for my latest requirement...
I need to collect fast A to D samples (from an external 8 bit A to D)... every 20ns.
Is it possible to use an 8 Bit parallel port and save 256 bytes into main memory using MDMA clocked using an external 50MHz source?
Thanks
Rick
2018-05-03 10:35 AM
For synchronous parallel input look at the camera interface DCMI. Should support rates north of 50 MHz. Also see FIFO devices.
Not really a DRQ/DACK model in STM32. You can use FSMC, or block of GPIO, and trigger DMA via TIM CHx input pin.
2018-05-04 12:13 AM
Thanks Clive,
I did consider that but have no experience of using it. I want to have a first hit production on this PCB so may get a development board in and try it, thanks. Like you say I could supply the clock and also use it for the DMA Trigger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.