STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 4.23.0 syscalls.c bugs ?

Posted on October 28, 2017 at 14:31Hi,i'm using STM32CubeMX V 4.23.0 to build a project for a stm32f107vct with FatFs, LWIP & FreeRTOS using the gcc-arm-none-eabi-6-2017-q2-update toolchain.Compiling the generated syscalls.c fails due various errors...

Unknown type for CanTxMsgTypeDef

Posted on May 03, 2018 at 08:39Hello,I have a similar code, where I define a message buffer of type CanTxMsgTypeDef. However, when compiling, I get an error saying  CanTxMsgTypeDef is an unknown type. So I guess this needs to be defined somewhere, o...

Eclipse Makefile error

Posted on May 04, 2018 at 10:03I got a error message - make: *** [test.elf] Error 1 when I build a project in Eclipse.Is there any way to solve this problem?.MCU : STM32F091RCT6Eclipse version : Neon.3 Release (4.6.3)Toolchain : Cross ARM GCC Buildi...

Resolved! NUCLEO-L496ZG-P - Keil support?

Posted on May 03, 2018 at 21:38Hi,I know it's rather a question to Keil but maybe someone came across this issue.The uVision cannot find STM32L496ZGTxP MCU when the IDE starts.  The current DFP is 2.0.0 (2017-10-06).I ignored the warning and success...

STM32x MDMA maximum Clock speed

Posted on May 03, 2018 at 16:44I have developed dozens of products using the STM32 Family, but can not find an easy solution for my latest requirement...I need to collect fast A to D samples (from an external 8 bit A to D)... every 20ns.Is it possib...

STM32F413 SPI with DMA safety

Posted on May 04, 2018 at 09:11Hi,We are using 2 STM32F413 controllers which are communicationg via the SPI peripheral along with DMA. Ours is a safety critical project we need to add some checks to the DMA as mentioned in the 'UM1840 User manual' -...

sushanth by Associate
  • 870 Views
  • 0 replies
  • 1 kudos

Scanf-Retarget Problem

Posted on November 14, 2011 at 11:51 Hello Forum! While trying to retarget the printf() and scanf() functions, with printf everything worked well.  However, with scanf occured a weird problem. First here are the overwrited low-level functions : siz...

Resolved! STM32F0 TIMx gate mode channel selection

Posted on May 02, 2018 at 20:48I'm using the gate mode TIM scheme as detailed in the reference manual:TIM3->CCMR1 |= TIM_CCMR1_CC1S_0; /* (1)*/ TIM3->CCER |= TIM_CCER_CC1P; /* (2) */ TIM3->SMCR |= TIM_SMCR_SMS_2 | TIM_SMCR_SMS_0 | TIM_SMCR_TS_2 | TI...

Resolved! TIM2 Upcounting Count Restart Issue

Posted on May 02, 2018 at 03:43The TIM2 timer on an STM32F0 seems to not be resetting to 0 once the counter reaches the ARR value on occasion. I am periodically changing the ARR value, but the values are all in a small range. After a random amount o...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.