2025-10-09 5:12 PM
Hi,
I am currently developing a small application with a STM32U5 where I write a few bytes into flash using HAL_FLASH_Program(). All seems to work fine. Except I can only read the data back after I do a reset. I suspect that DCACHE is playing a trick on me? But I am not sure how to invalidate the DCache (preferably only for a small section)
SCB_InvalidateDCache();Seems to have some problems on the STM32U5? At least, I was unable to include the prober h-file w/o getting tons of errors.
What is the new strategy for cache invalidation?
Thanks,
Juergen
2025-10-09 5:16 PM
SCB_InvalidateDCache or SCB_InvalidateDCache_by_Addr are the correct ways to invalidate a section of memory. What problems are you running into? Should be able to call those with code generated from an IOC file by STM32CubeMX.
2025-10-09 5:24 PM
Thanks for your VERY quick reply.
What file do i need to include?
I tried directly in main.c (code generated from IOC file):
../Core/Src/main.c:385:3: error: implicit declaration of function 'SCB_InvalidateDCache' [-Werror=implicit-function-declaration]
385 | SCB_InvalidateDCache();
| ^~~~~~~~~~~~~~~~~~~~I once used a STM32H7, there everything worked fine. But the STM32U5 and the departure from CMSIS are making things a bit harder :)
Thanks,
Juergen
2025-10-09 6:18 PM - edited 2025-10-09 6:19 PM
What chip do you have? Are you starting from an IOC file?
In a random STM32U5 chip, the compiler has no problem with "SCB_InvalidateDCache" for me.
2025-10-10 2:04 AM
Hi,
for completion, I figured it out.
HAL_StatusTypeDef HAL_DCACHE_InvalidateByAddr(DCACHE_HandleTypeDef *hdcache, const uint32_t *const pAddr, uint32_t dSize)is the new Api to use. But apparently, if you write to flash Dcache is not the correct cache for that? What works for me is:
HAL_ICACHE_Invalidate();Apperently Icache is responsible for that (at least AI tells me?).
I had success by removing all Dcache but not for specific memory areas which caught my suspicias/unsatisfied. I expect that beeing not correct.
HAL_DCACHE_Invalidate(&hdcache1);Can anybody shed some light here?
Thanks,
Juergen
2025-10-10 9:56 AM
ICACHE isn't relevant unless you are changing instruction code, which is not likely.
Didn't see answers to any of my questions.
2026-03-21 3:34 AM
Not OP but I ran into the same problem with STM32U5A5QJI.
After writing to flash memory, my validate function that compares RAM and flash immediately afterwards kept failing despite the RAM and flash memory contents being identical.
It was failing with memcmp and even a simple for loop comparing byte by byte.
It was only resolved after adding a call to HAL_ICACHE_Invalidate(); before running the comparison function.
I suspect the ICACHE doesn't care about flash being used for data and therefore it's the ICACHE that needs to be flushed after flash operations.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.