2019-06-07 6:05 AM
Dear all,
I am facing to a strange GPIO problem. First af all, I tried to set-up the LPUART1 but impossible to send anything (no activity on PG7 , the Tx of the LPUART1). So, I initialized the PG7 to be a general output and tried to blink it ... no reaction. With the scope I noticed that the pin remain in Z impedance. I tried the same exercise on PG0 and PG1; this work as expected . All the other PGx (that are not connected to special functions of the board) do not change their output. On the other ports (A, B, C ...) I have no problem. Any idea? Do I need some special initialization for this port G? here is ma simple code I used for those basic tests:
static void myTest(void) {
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; // Turn on the GPIOA
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; // Turn on the GPIOB
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOCEN; // Turn on the GPIOC
RCC->AHB2ENR |= RCC_AHB2ENR_GPIODEN; // Turn on the GPIOD
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOEEN; // Turn on the GPIOE
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOFEN; // Turn on the GPIOF
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOGEN; // Turn on the GPIOG
// Example for PG7
GPIOG->AFR[0] = (0xF<<28); // AF15
GPIOG->OSPEEDR = (0x3<<14); // Very high speed
GPIOG->OTYPER = (0x0<<14); // Push-pull
GPIOG->MODER = (0x1<<14); // Output
GPIOG->PUPDR = (0x0<<14); // No pull-up
GPIOG->ODR |= (0x0<<7); // Initial value
while (TRUE) {
GPIOG->ODR |= (1<<7);
GPIOG->ODR &= ~(1<<7);
}
}
Thank you for your suggestions,
BR, Edo
Solved! Go to Solution.
2019-06-08 6:43 AM
/* IOSV bit MUST be set to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
SET_BIT(PWR->CR2, PWR_CR2_IOSV);
or
/* VddIO2 must be enabled to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddIO2();
__HAL_RCC_GPIOG_CLK_ENABLE();
2019-06-08 4:03 AM
With a debugger, stopp in your loop. Read the GPIOG registers and interpret the setting.. Set them by hand and check ODR, IDR and the actual pin state. I did not see any remark around GPIOG in the datasheet, the reference manual or the errata. So there is high propability that your code is not right. Report back!
2019-06-08 4:36 AM
Also check the schematics for PG7, maybe there is something tied there.
2019-06-08 6:31 AM
You need to explicitly power the GPIOG bank, there is a specific PWR/VDDIO2 setting.
2019-06-08 6:43 AM
/* IOSV bit MUST be set to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
SET_BIT(PWR->CR2, PWR_CR2_IOSV);
or
/* VddIO2 must be enabled to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddIO2();
__HAL_RCC_GPIOG_CLK_ENABLE();
2019-06-09 12:31 AM
All, thank you for your help.
The good answer is the Clive one.
Unfortunately, in the ST documentation this point is explicitly mentioned only in the PWR chapter. As the primary function is related to the GPIO, I would expect a more explicit notice about this special PWR setting for the port G [2..15] even in the GPIO chapter.
Now my program works like a charm.
Thank's
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.