STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407VET6 remap CAN1

Hi,I use CubeMX for STM32F407VET6.I want to remap CAN1 pins for PB8, PB9, but that configuration initialzing with error.Though CAN1 remap for PD0, PD1 is fine.What does that mean?Thank you very much in advance for your return guys!

ADry by Associate II
  • 1298 Views
  • 2 replies
  • 0 kudos

H750 vs H743 for QuadSPI Boot

Hello guys!I'm working on a custom board with STM32H750VB and a Winbond QuadSPI flash. The ideia is boot the code from QSPI as H750 program memory is a little low. I'm also working with STM32H743VI on a twin custom board, so I can create and debug th...

Peaga by Senior
  • 4894 Views
  • 12 replies
  • 0 kudos

About usart in stm32?

I coded for usart communication in stm32f103r8.In this i'm getting the garbage value as output.given below is my program,kindly help me to correct my program.****#include "stm32f10x.h"#include "stm32f10x_usart.h"void usartSetup (void);int SendChar ()...

Sm.16 by Associate II
  • 7146 Views
  • 16 replies
  • 0 kudos

POR via STLink

Hi,How can I power cycle the Nucleo-144 between debug sessions with out unplugging and reinserting the USB cable. Is there a way to toggle PWR_ENn on the STLINK using openOCD and if so could someone please post the script that does this?thank you

JButl by Associate
  • 827 Views
  • 0 replies
  • 0 kudos

Resolved! I2c device never sets SB bit after start is transmitted.

My MPU is STM32L152RET6I am using i2c channel 1 to communicate with an i2c device.  I used the standard device set and verified the hardware appears to be set up correctly. When I set the "Start" bi in control register 1 (CR1), a start condition is g...

TSchm by Associate
  • 2463 Views
  • 1 replies
  • 0 kudos

Program gets vanished after reboot or reset

I am using custom board with STM32F779BI. Its works fine while debugging using ST-LINK V2, But after reset or reboot program gets vanished. Didnt work after reset. Is there problem with debug configuration? or something else?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.