2024-12-11 3:08 AM
I have a strange problem
I use sloeber, an eclipse arduino "plugin" and up to now that worked fine.
Now I wanted to debug a custom STM32L412KB board and I can't connect to the MCU.
I always get an error message that the MCU cannot be found
xPack Open On-Chip Debugger 0.12.0+dev-01557-gdd1758272-dirty (2024-04-02-07:27)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Started by GNU MCU Eclipse
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 500 kHz
Info : STLINK V2J43M28 (API v2) VID:PID 0483:374B
Info : Target voltage: 3.242904
Error: init mode failed (unable to connect to the target)
the debugger is a STM32L4R5 eval board
but connecting/erasing/flashing with STM32CubeProgrammer works fine with the very same setup
I use the same SW stack to debug custom STM32L4R5 boards, but this time with a STLINK-V3MINIE
I am not familiar with GDB/openOCD, up to now it just worked almost out of the box
any hint appreciated!
2024-12-20 4:13 AM
Hello @b.a.
Make sure to upgrade your firmware and use latest release of STM32CubeProgrammer.
Check your connectivity pins and jumper on the board and try "Connect Under Reset" mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.