2018-06-20 3:57 PM
Hi,
I am working on STM32 flash program using a sample program from V1.11. The program is pretty straight forward. Erase ADDR_FLASH_PAGE_16 to ADDR_FLASH_PAGE_255 then program.
The program stuck in HardFault_Handler doing HAL_FLASHEx_Erase in the first page erase FLASH_PageErase(page_index, pEraseInit->Banks);
HAL_FLASH_Program()
also failed on FLASH_Program_DoubleWord().Anyone experienced same issue? Doesn't this supposed to be working without any changes?
Thx
STM32Cube_FW_L4_V1.11.0\Projects\NUCLEO-L496ZG\Examples\FLASH\FLASH_EraseProgram
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
{ while (1) { BSP_LED_On(LED3); } }Address = FLASH_USER_START_ADDR;
while (Address < FLASH_USER_END_ADDR) { if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, DATA_64) == HAL_OK) { Address = Address + 8; } else { /* Error occurred while writing data in Flash memory. User can add here some code to deal with this error */ while (1) { BSP_LED_On(LED3); } } }HAL_FLASH_Lock();
Address = FLASH_USER_START_ADDR;
MemoryProgramStatus = 0x0;while (Address < FLASH_USER_END_ADDR)
{ data32 = *(__IO uint32_t *)Address;if (data32 != DATA_32)
{ MemoryProgramStatus++; } Address = Address + 4; }/*Check if there is an issue to program data*/
if (MemoryProgramStatus == 0) { /* No error detected. Switch on LED1*/ BSP_LED_On(LED1); } else { /* Error detected. Switch on LED2*/ BSP_LED_On(LED2); }2018-06-21 12:52 PM
>> Seems working. Why?
Perhaps you're not erasing code that is executing? Perhaps there is something else going on?
May be you can do some analysis and debugging to pin point why you get failures?
If the software Hard Faults, it is typically because the processor is being asked to touch some address it shouldn't, or you're attempting to execute broken/missing code.
Things I normally do when testing examples : 1) Add code to output printf() via SWV or USART, 2) Have a Hard Fault Handler that outputs diagnostic messages about internal register states should it fault. This allows me to quickly determine what's going on inside the black box.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.