2018-06-21 1:56 AM
I am running STM32F303VC.
I require an IRQ on GPIOE_Pin_15 ---> TIM2_Channel_1
My typical Frequency range is from 5 Hz - 500Hz
This is required to provide me with a number of ticks between the 2 interrupts. The result is then passed to TIM3 /100
PreScaler = Same for both timers
TIM2_Period = 1
TIM3_Period = Result / 100
TIM3 then provides me with 100 points between the original to trigger other events an certain points.
The problem I am having is the IRQ_Handlers do not get triggered.
I have monitored the GPIO_Pin_15 through a while loop and confirm this is toggling, however TIM2 doe not update TIM3 and TIM3 does NOT output either.I can provide my Main.C file if you email me
mailto:kim@accesssecurity.co.nz
#stm32f3 #timer-interrupt2018-06-21 8:01 AM
The problem I am having is the IRQ_Handlers do not get triggered.
Read back the content of relevant GPIO and TIM (and NVIC) registers and
- check if AF is set for given pin in GPIO_MODER
- check if the proper AF is selected in GPIO_AFRL/AFRH
- check if input capture is set in TIMx_CCMRy
- check if channel enabled in TIMx_ENR
- check if interrupt for that channel enabled in TIMx_DIER
- check if interrupt for that timer is enabled in NVIC
- check if the ISR name matches that in the vector/startup file(keep in mind name mangling if you compile as C++) (check in disassembled binary perhaps)
JW
2018-06-21 8:09 AM
'
The problem I am having is the IRQ_Handlers do not get triggered.'
yeah. but the problem isn't with your code. so look somewhere else, please.
2018-06-21 1:02 PM
Indeed, there's no such AF on that pin... I didn't realize the OP didn't care to check...
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.