2017-02-10 7:55 AM
Hi,
I'm trying to communicate with
http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1761.pdf
via SAI, STM32L476 is master. I sucessfully connected to it via I2C, now I need to send data. I dont have much experience with SAI. The task is to play22.05kHz
16 bit WAVE and also record audio. I usedSAI2A for RX, SAI2B for TX, 4 pins mode (ADC_SDATA - SAI2_SD_A, DAC_SDATA - SAI2_SD_B, LRCLK - SAI2_FS_A, BCLK - SAI2_SCK_A)
. I saw guide but instead of using SAI2A for TX I use it for RX. As far I as understood ADAU1761 needs MCLK to record/play audio. When I use HAL_SAI_Transmit() the MCLK is not generated, I checked it with logic analyzer. However with HAL_SAI_Receive() MCLK is present. Is there any way to generate MCLK duringHAL_SAI_Transmit()
with this configuration? Maybe somebody has some experience with interfacing STM32 and ADAU17xx or ADAU14xx DSPs. Here is my configuration:void MX_SAI2_Init(void)
{hsai_BlockA2.Instance = SAI2_Block_A;
hsai_BlockA2.Init.Protocol = SAI_FREE_PROTOCOL; hsai_BlockA2.Init.AudioMode = SAI_MODEMASTER_RX; hsai_BlockA2.Init.DataSize = SAI_DATASIZE_16; hsai_BlockA2.Init.FirstBit = SAI_FIRSTBIT_MSB; hsai_BlockA2.Init.ClockStrobing = SAI_CLOCKSTROBING_FALLINGEDGE; hsai_BlockA2.Init.Synchro = SAI_ASYNCHRONOUS; hsai_BlockA2.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockA2.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE; hsai_BlockA2.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF; hsai_BlockA2.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_22K; hsai_BlockA2.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockA2.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockA2.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockA2.FrameInit.FrameLength = 32; hsai_BlockA2.FrameInit.ActiveFrameLength = 16; hsai_BlockA2.FrameInit.FSDefinition = SAI_FS_CHANNEL_IDENTIFICATION; hsai_BlockA2.FrameInit.FSPolarity = SAI_FS_ACTIVE_LOW; hsai_BlockA2.FrameInit.FSOffset = SAI_FS_FIRSTBIT; hsai_BlockA2.SlotInit.FirstBitOffset = 0; hsai_BlockA2.SlotInit.SlotSize = SAI_SLOTSIZE_DATASIZE; hsai_BlockA2.SlotInit.SlotNumber = 2; hsai_BlockA2.SlotInit.SlotActive = 0x00000003; if (HAL_SAI_Init(&hsai_BlockA2) != HAL_OK) { Error_Handler(); }hsai_BlockB2.Instance = SAI2_Block_B;
hsai_BlockB2.Init.Protocol = SAI_FREE_PROTOCOL; hsai_BlockB2.Init.AudioMode = SAI_MODESLAVE_TX; hsai_BlockB2.Init.DataSize = SAI_DATASIZE_16; hsai_BlockB2.Init.FirstBit = SAI_FIRSTBIT_MSB; hsai_BlockB2.Init.ClockStrobing = SAI_CLOCKSTROBING_FALLINGEDGE; hsai_BlockB2.Init.Synchro = SAI_SYNCHRONOUS; hsai_BlockB2.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockB2.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF; hsai_BlockB2.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockB2.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockB2.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockB2.Init.TriState = SAI_OUTPUT_NOTRELEASED; hsai_BlockB2.FrameInit.FrameLength = 32; hsai_BlockB2.FrameInit.ActiveFrameLength = 16; hsai_BlockB2.FrameInit.FSDefinition = SAI_FS_CHANNEL_IDENTIFICATION; hsai_BlockB2.FrameInit.FSPolarity = SAI_FS_ACTIVE_LOW; hsai_BlockB2.FrameInit.FSOffset = SAI_FS_FIRSTBIT; hsai_BlockB2.SlotInit.FirstBitOffset = 0; hsai_BlockB2.SlotInit.SlotSize = SAI_SLOTSIZE_DATASIZE; hsai_BlockB2.SlotInit.SlotNumber = 2; hsai_BlockB2.SlotInit.SlotActive = 0x00000003; if (HAL_SAI_Init(&hsai_BlockB2) != HAL_OK) { Error_Handler(); }}
DMA SAI2A init:
hdma_sai2_a.Instance = DMA1_Channel6;
hdma_sai2_a.Init.Request = DMA_REQUEST_1; hdma_sai2_a.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_sai2_a.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai2_a.Init.MemInc = DMA_MINC_ENABLE; hdma_sai2_a.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_sai2_a.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_sai2_a.Init.Mode = DMA_CIRCULAR; hdma_sai2_a.Init.Priority = DMA_PRIORITY_HIGH;DMA SAI2B init:
hdma_sai2_b.Instance = DMA1_Channel7;
hdma_sai2_b.Init.Request = DMA_REQUEST_1; hdma_sai2_b.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_sai2_b.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai2_b.Init.MemInc = DMA_MINC_ENABLE; hdma_sai2_b.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_sai2_b.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_sai2_b.Init.Mode = DMA_CIRCULAR; hdma_sai2_b.Init.Priority = DMA_PRIORITY_HIGH;#stm32 #stm32l4 #stm32-sai #sai2017-02-11 8:12 AM
OK, The answer is simple. I need to call
HAL_SAI_Receive_DMA(&hsai_BlockA2, saiRxBuff, 512);
HAL_SAI_Transmit_DMA(&hsai_BlockB2, saiTxBuff, 512);and the MCLK is generated during SAI2B transmission.
2017-02-14 7:56 AM
Ok, I'm confused about MCLK. Datasheet says that MCLK = (sampling rate * 256). However if I use CubeMX and generate code for 48kHz sampling rate the MCLK should be 12,288MHz. In clock configuration tab I can choose SAI2 clock source and speed. I choosed PLLSAI2P = 24MHz, there is 12MHz on the output. I checked it with logic analyzer and it looks like this:
Any idea why?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.