2025-02-12 10:16 PM - last edited on 2025-02-14 5:52 AM by mƎALLEm
Hello, I am working on the STM32L476RG MCU, where I first measure the angle using the atan2 function and then convert this measured angle into UVW signals.
As we know, UVW signals are digital in nature, switching high/low based on conditions specified in the code. For this, I used digital pins 8, 9, and 10 as GPIO output pins.
However, I observed that pins 9 and 10 provide the expected output, but pin 8 remains constantly high.
Why is this happening? I am sharing my code with you—please check it once
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc2;
DAC_HandleTypeDef hdac1;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_ADC2_Init(void);
static void MX_DAC1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_ADC2_Init();
MX_DAC1_Init();
/* USER CODE BEGIN 2 */
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc2, 1);
raw_sin=HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
HAL_ADC_Start(&hadc2);
HAL_ADC_PollForConversion(&hadc1, 1);
raw_cosin=HAL_ADC_GetValue(&hadc2);
HAL_ADC_Stop(&hadc2);
vsin=(raw_sin*(3.3/4095)-1.721);
vcos=(raw_cosin*(3.3/4095)-1.7465);
angle=atan2(vsin,vcos);
angle=angle*(180.0f/M_PI);
if(angle < 0)
angle+=180;
dac_val=(uint32_t)((angle/180)*4095.0f);
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, dac_val);
//for(angle=0;angle<360;angle++)
//{
if(angle >=0 && angle <60)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 1);
}
else if(angle >= 60 && angle <120)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 0);
}
else if(angle >= 120 && angle <180)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 0);
}
else if(angle >= 180 && angle <240)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 0);
}
else if(angle >= 240 && angle <300)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 1);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 1);
}
else if(angle >= 300 && angle <360)
{
HAL_GPIO_WritePin(UVW_PORT, U_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, 0);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, 1);
}
}
/*if (angle >= 0 && angle < 60) {
GPIOA->BSRR = (1U << | (1U << (10)); // U = HIGH, W = HIGH
GPIOA->BSRR = (1U << (9 + 16)); // V = LOW
}
else if (angle >= 60 && angle < 120) {
GPIOA->BSRR = (1U << 8); // U = HIGH
GPIOA->BSRR = (1U << (9 + 16)) | (1U << (10 + 16)); // V = LOW, W = LOW
}
else if (angle >= 120 && angle < 180) {
GPIOA->BSRR = (1U << | (1U << 9); // U = HIGH, V = HIGH
GPIOA->BSRR = (1U << (10 + 16)); // W = LOW
}
else if (angle >= 180 && angle < 240) {
GPIOA->BSRR = (1U << 9); // V = HIGH
GPIOA->BSRR = (1U << (8 + 16)) | (1U << (10 + 16)); // U = LOW, W = LOW
}
else if (angle >= 240 && angle < 300) {
GPIOA->BSRR = (1U << 9) | (1U << 10); // V = HIGH, W = HIGH
GPIOA->BSRR = (1U << (8 + 16)); // U = LOW
}
else if (angle >= 300 && angle < 360) {
GPIOA->BSRR = (1U << 10); // W = HIGH
GPIOA->BSRR = (1U << (8 + 16)) | (1U << (9 + 16)); // U = LOW, V = LOW
}*/
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 10;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief Peripherals Common Clock Configuration
* @retval None
*/
void PeriphCommonClock_Config(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC;
PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_PLLSAI1;
PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSI;
PeriphClkInit.PLLSAI1.PLLSAI1M = 1;
PeriphClkInit.PLLSAI1.PLLSAI1N = 8;
PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV7;
PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV2;
PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV2;
PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_ADC1CLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief ADC1 Initialization Function
* None
* @retval None
*/
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_MODE_INDEPENDENT;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
/**
* @brief ADC2 Initialization Function
* None
* @retval None
*/
static void MX_ADC2_Init(void)
{
/* USER CODE BEGIN ADC2_Init 0 */
/* USER CODE END ADC2_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC2_Init 1 */
/* USER CODE END ADC2_Init 1 */
/** Common config
*/
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc2.Init.LowPowerAutoWait = DISABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc2.Init.DMAContinuousRequests = DISABLE;
hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc2.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC2_Init 2 */
/* USER CODE END ADC2_Init 2 */
}
/**
* @brief DAC1 Initialization Function
* None
* @retval None
*/
static void MX_DAC1_Init(void)
{
/* USER CODE BEGIN DAC1_Init 0 */
/* USER CODE END DAC1_Init 0 */
DAC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN DAC1_Init 1 */
/* USER CODE END DAC1_Init 1 */
/** DAC Initialization
*/
hdac1.Instance = DAC1;
if (HAL_DAC_Init(&hdac1) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT1 config
*/
sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_ENABLE;
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DAC1_Init 2 */
/* USER CODE END DAC1_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
// HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10, GPIO_PIN_RESET);
/*Configure GPIO pins : PA8 PA9 PA10 */
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_WritePin(UVW_PORT, U_PIN, GPIO_PIN_RESET);
HAL_GPIO_WritePin(UVW_PORT, V_PIN, GPIO_PIN_RESET);
HAL_GPIO_WritePin(UVW_PORT, W_PIN, GPIO_PIN_RESET);
// Enable GPIOA clock
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
// // Set PA8, PA9, PA10 as outputs
// GPIOA->MODER &= ~(3U << (8 * 2)); // Clear bits for PA8
// GPIOA->MODER |= (1U << (8 * 2)); // Set as output
//
// GPIOA->MODER &= ~(3U << (9 * 2));
// GPIOA->MODER |= (1U << (9 * 2));
//
// GPIOA->MODER &= ~(3U << (10 * 2));
// GPIOA->MODER |= (1U << (10 * 2));
//
// GPIOA->BSRR =(1U <<(8+16)) | (1U <<(9+16)) | (1U << (10+16));
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2025-02-13 6:08 AM
HAL_GPIO_WritePin is the correct call to change the value of an output pin. There are a few possibilities here:
2025-02-13 10:10 PM
Sir, I have checked everything as you suggested, but the problem still persists.
2025-02-13 10:33 PM
Write to that pin in the code before the loop and check that the output can switch level.
Set a breakpoint at the place in the loop where you expect the pin to be switched and check if your code hits this breakpoint.
hth
KnarfB
2025-02-13 11:58 PM
Hi sir, as per your suggestion, I implemented the code. Before the loop, I reset all pins and also applied a breakpoint. I observed that two pins are working fine, but the U pin is always high and does not change at any point.
2025-02-14 5:44 AM
Maybe the pin is damaged.
Show the contents of the GPIOA registers after setting all 3 pins push-pull output and output high.
2025-02-18 3:40 AM
sir i checked with all these parameters but not getting solution .any other solution sir.
2025-02-19 8:55 AM
Before your while(1), just toggle the pins high with delay to see if the pins change or not. If not changing, disconnect all external circuit and toggle.
2025-02-19 10:41 AM - edited 2025-02-19 10:43 AM
angle=atan2(vsin,vcos); angle=angle*(180.0f/M_PI); if(angle < 0) angle+=180;
This results in angle being always between 0 and 180, so in subsequent code the legs where U would be cleared are never executed.
You probably wanted to add 360 rather than 180.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.