2017-12-12 12:10 AM
Hi everyone,
I'm using all ADC modules ADC1, ADC2, and ADC3 in my application. ADC1 has 8 channels so the data is being read through DMA.
Others which are ADC2 and ADC3 have only 4 channels and I want them to be read in Injected mode. However, both of them read zero
data
while reading in Injected mode.Furthermore, while trying to read the second time I get an error, it says it's busy. Where am I doing wrong?
if(HAL_ADCEx_InjectedStart(&hadc2)!=HAL_OK)
Error_Handler();
HAL_ADCEx_InjectedPollForConversion(&hadc2,100);
usAdc[0]=HAL_ADCEx_InjectedGetValue(&hadc2,ADC_INJECTED_RANK_1);
usAdc[1]=HAL_ADCEx_InjectedGetValue(&hadc2,ADC_INJECTED_RANK_2);
usAdc[2]=HAL_ADCEx_InjectedGetValue(&hadc2,ADC_INJECTED_RANK_3);
usAdc[3]=HAL_ADCEx_InjectedGetValue(&hadc2,ADC_INJECTED_RANK_4);
#injected-adc #injected-conversionWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.