STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Main application running at address 0x08040000

Posted on December 11, 2017 at 20:34Hi,I'm using a STM32F417 on which I want to have a bootloader (at the beginning of the flash, i.e. address 0x08000000) and two applications using FreeRTOS (one at address 0x08004000 and the other one at address 0x...

Analog watchdog not working after calibration

Posted on December 12, 2017 at 16:40Dear ST users, I want to get an Analog Watchdog interrupt after the VrefInt value exceeds the window thresholds. I configured everything using STMCUBE. The interrupt works fine only it is very inaccurate.  When I ...

NUCLEO F767ZI draws far more current than 300mA , it's overcurrent LD5 keeps on glowing even when no load is connected and U4 gets very hot.Anyone know what could be causing them ? Is there any fix for it.

Posted on December 07, 2017 at 08:39https://community.st.com/tags♯/?tags=nucleo-f767zi‌https://community.st.com/tags♯/?tags=x-nucleo-idw01m1%3B%20nucleo-f767zi‌https://community.st.com/tags♯/?tags=f767zi%3B‌♯‌#x-nucleo-idw01m1

SPI clock frequency in STM32F769NI Disco board

Posted on December 12, 2017 at 06:35how to configure for SPI clock frequency in SPI example provided.Example give below i am usingIn atmel board we are using 5mhz or 50khz SPI clock frequency.int main(void){  /* Enable the CPU Cache */  CPU_CACHE_En...

STM32F030 changing deadtime under operation

Posted on December 11, 2017 at 21:37Hello Community.I have a project with PWM output TIM1_CH2 and TIM1_CH2N.I can set deadtime without problem if I do that at the inicialization and setting the TIM1_BDTR lock_level_1.But I want to change the deadtim...

Balint C by Associate
  • 1553 Views
  • 1 replies
  • 0 kudos

Seconds in RTC is jumping

Posted on December 11, 2017 at 13:51Hello, I am developing a motor controller using STM32F407, I wrote the code for RTC and uploaded it. I found the time jumps seconds (2 or 3 seconds each time). RTC is crucial in my project as I have to control the...

STM32L476 Adc Injected

Posted on December 12, 2017 at 09:10Hi everyone,I'm using all ADC modules ADC1, ADC2, and ADC3 in my application. ADC1 has 8 channels so the data is being read through DMA.Others which are ADC2 and ADC3 have only 4 channels and I want them to be rea...

How can STM32F446RE connect external SDRAM

Posted on December 04, 2017 at 21:23The data sheet says there is no FMC on STM32F446RE. Is that means there is no chance to connect external RAM with STM32F446RE?#stm-32 #external-ram #stm32f446re

Qiyan Li by Associate
  • 1178 Views
  • 1 replies
  • 0 kudos

Resolved! LCD1602 + pcf8574 (I2C) + STM32F0

Posted on October 21, 2017 at 21:04Hello.I have some problem with LCD1602+pcf8574 (I2C) and STM32F0. I experience the following bugs1) When I try to display more than three symbols they seem to be ignored2) If I try to display three symbols, I have ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.