2026-04-10 4:06 PM
I am working on a project in which the sensor data that will calculated by stm32 will be sent via using the esp32 as a wifi module to aws , now the problem is i have inserted the stm32 and esp32 inside a pcb with the required circuit connection but i am having difficulty flashing the code to esp32 or connecting to esp32 , i have tried various methods but cant seem to find a solution.
thing is the code cannot be flashed directly to esp32 , it has to be sent via stm32 due to circuit connections and no availability of usb connection ?
current status right now:-
i am using the process of semihosting to flash the code into stm32 and get results on the serial monitor since i dont have a usb connection for stm32 , i am using the st link of nucleo externally , if someone can help me regarding conversion of my stm32l476 to a bridge to flash code on esp32 or to convert esp32 to wifi module ,it would be very helpful ,this is the last step after this only calibration is required to complete my project.
2026-04-11 12:42 PM
2026-04-13 5:16 AM
To program the ESP32, semihosting is not recommended. Semihosting is a debug I/O feature for the STM32, while ESP32 flashing requires a programming path such as UART bootloader mode with control of EN and GPIO0 pins. If those ESP32 pins are not accessible on the PCB, a hardware or wiring change is required.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-13 5:26 AM
@MaddyGitBase wrote:the code cannot be flashed directly to esp32 , it has to be sent via stm32 due to circuit connections and no availability of usb connection ?
Is that a question ?
@MaddyGitBase wrote:i am using the process of semihosting to flash the code into stm32 and get results on the serial monitor since i dont have a usb connection for stm32
Do you really mean Semihosting here? As @FBL said, Semihosting would not be a usual way to do this!
@MaddyGitBase wrote:help me regarding conversion of my stm32l476 to a bridge to flash code on esp32
So what have you done so far?
You'll need to research what options the ESP32 has for firmware updates; eg, a UART bootloader?
Does it not support OTA updates using its WiFi?
You'll need to go to an ESP32 and/or Espressif forum for that; eg, https://esp32.com/ - it's nothing to do with ST or STM32
@MaddyGitBase wrote:or to convert esp32 to wifi module.
Surely, an ESP32 is a WiFi module?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.