2021-09-07 1:59 AM
Could we used the SPI interface control the 5V LED Driver IC?
Is there anything that needs extra attention?
Will there be problems with SPI operation?
Solved! Go to Solution.
2021-09-07 2:56 AM
It should work, provided pins are correctly configured.
You need to ensure +5V is never applied when the chip is not powered (VDD=0).
What LED driver? Make sure that 3.3V is guaranteed to be logic high.
2021-09-07 2:56 AM
It should work, provided pins are correctly configured.
You need to ensure +5V is never applied when the chip is not powered (VDD=0).
What LED driver? Make sure that 3.3V is guaranteed to be logic high.
2021-09-07 5:57 PM
Hi TDK,
Thanks a lot.
The LED Driver is IS31FL3743B.
The Vih min is 2.4V.
2021-09-07 6:26 PM
Hi TDK,
About this question, does ST have any document for SPI operation @ 5V?
2021-09-07 6:44 PM
I don't think you'll find anything that specific. What are you looking to find out? The reference manual is typically the best source of information, followed by the datasheet for chip-specific things.
The SPI would be operating at the STM32's voltage, which is (typically) 3.3V. Only the MISO line would be 5V.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.