2017-09-22 6:45 AM
I am currently using the 'STM32CubeFunctionPack_MOTENV1_V3.0.0' for SensorTile platform.
I does support the USBD_cdc function in sending data to PC (Print) but missing the receive code.
Since there is a ST BLE on board, I would like to connect with the 'BlueNRG GUI' tools which I can perform firmware update through USB for ST-BLE.
1. Where I could find the example code for USBD receive for STM32L4 ?
2. Is 'BlueNRG DK 2.0.2\Projects\Projects_Cube\BlueNRG_Stack_IFR_Updater' be the right package to start ?
Thanks
2017-09-22 9:57 AM
Hi,
Have a look to the
firmware package to find the USB device example.You have the
https://community.st.com/0D50X00009XkffXSAR
Bluetooth Low Energy software expansion for STM32Cube, you can start with thesample applications in Projects\Multi\Applications and followthe instructions provides in thereadme.txt file to run the example.Best Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.