2016-06-18 11:23 AM
Hi,
change in the ''SPI_FullDuplex_ComDMA'' to work in 16bits mode.change in the ''stm32l4xx_hal_msp.c'' file://************************************************************** hdma_tx.Instance = SPIx_TX_DMA_CHANNEL; hdma_tx.Init.Request = SPIx_TX_DMA_REQUEST; hdma_tx.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_tx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_tx.Init.MemInc = DMA_MINC_ENABLE; hdma_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_tx.Init.MemDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_tx.Init.Mode = DMA_NORMAL; hdma_tx.Init.Priority = DMA_PRIORITY_LOW; HAL_DMA_Init(&hdma_tx); /* Associate the initialized DMA handle to the the SPI handle */ __HAL_LINKDMA(hspi, hdmatx, hdma_tx); /* Configure the DMA handler for Transmission process */ hdma_rx.Instance = SPIx_RX_DMA_CHANNEL; hdma_rx.Init.Request = SPIx_RX_DMA_REQUEST; hdma_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_rx.Init.MemDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_rx.Init.Mode = DMA_NORMAL; hdma_rx.Init.Priority = DMA_PRIORITY_HIGH; HAL_DMA_Init(&hdma_rx);//***********************************************************Change in the main.c file://**************************************************************** SpiHandle.Instance = SPIx; SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; SpiHandle.Init.Direction = SPI_DIRECTION_2LINES; SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE; SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW; SpiHandle.Init.DataSize = SPI_DATASIZE_16BIT; SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB; SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE; SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; SpiHandle.Init.CRCPolynomial = 7; SpiHandle.Init.CRCLength = SPI_CRC_LENGTH_8BIT; SpiHandle.Init.NSS = SPI_NSS_SOFT; SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; sTxBuf[0] = 0x54C2; if(HAL_SPI_TransmitReceive_DMA(&SpiHandle, (uint8_t *)&sTxBuf[0], (uint8_t *)aRxBuffer, 1) != HAL_OK) { Error_Handler(); } If the the length field is 1, like above. SPI line transmit 16 bits: 00C2 If the length is 2, SPI line trasmit 32 bits: 00C20054. If I use: HAL_SPI_Transmit(&SpiHandle, (uint8_t*) &sTxBuf[0], 1,10); SPI line transmit correctly: 0x54C2 I tried the same with the STM32F303RE and it transmits correctly in 16 bits using DMA or not. Should it be some bug in the STM32L4 hardware? //****************************************************************2016-06-18 12:49 PM
PDATA?
2016-06-18 3:13 PM
clive1, what is PDATA?
the sTxBuf is 16 bits. And I would like to reiterate that the L4 transmits correctly in 16 bits without DMA, and the STM32F303 trasmits correctly with and without DMA, using the same setup.Ari.2016-06-18 5:04 PM
Peripheral Data, you should search your code and review your application of it.
Observation#2DMA_PDATAALIGN_HALFWORD != DMA_MDATAALIGN_HALFWORD2016-06-20 9:30 AM
2023-06-20 5:09 AM
Thank you so much, I had the same problem and I was pulling my hair out for over a week! Of course it was a copy-paste mistake :D
2023-06-20 5:39 AM
What often helps in these cases - as it both breaks the "author's blindness", and also helps to refresh the intimate knowledge of the mcu's internals - is to read out content of related registers and check against description of all individual field in those registers' descriptions in RM.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.