2017-04-07 1:27 AM
Hello everybody,
I have the following situation:
My question now is:
What I found out so far:
2017-04-07 1:29 AM
Pardon me for the bad manners - I pressed Enter to soon. Here is the proper ending of my post:
Hope you can help me with my problem.
Kind regards
Markus
2017-04-07 2:04 AM
For the 'L4 DMA, probably AN2548 is appropriate, even if it talks about F1/L1 - I believe the DMA in 'L4 is the same/similar than that in 'F1/'L1/'F0/'L0 (and quite different from that found in 'F2/'F4/'F7). However, the total transfer time calculation is not trivial and in your case might be quite different from what's given there, as:
- there may be simpler/shorter arbitration within the DMA if only one channel is used
- there may be simpler/shorter arbitration on the AHB/APB bridge if the AHB/APB clock is 1:1
- there may be simpler/shorter arbitration on the bus matrix if processor won't access the shared resources (SRAM, APB) ever
It may quite well be that you've already found the sweet spot.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.