STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupts Vector Table

Posted on April 03, 2017 at 19:00Hi,I am using STMF103R8. I developed a bootloader, which jump to main application. Everything works fine.Because I made two programs: one for the bootloader and one for the application, I see that the flash is progra...

sirpak by Associate II
  • 9718 Views
  • 6 replies
  • 0 kudos

STM32L4 DMA latency for ADC to SRAM transfer

Posted on April 07, 2017 at 10:27Hello everybody,I have the following situation: Processor STM32L47648MHz HSEI want to sample an external signal at 4MSPS. Therefore I use 60MHz PLLSAI1 as ADC1's clockThis gives 4MSPS (with 2.5cycles sampling and 12...

SPI Master Read Write using HAL commands

Posted on March 31, 2017 at 04:56Hi All,   I am new to STM , I  have problem in  read and write data simultaneously  using STM32L476 board. i just created a new project using STMcubeMX and try to read and write  simultaneously  using HAL_SPI_Transmi...

Pros and Cons of using CubeMx

Posted on April 06, 2017 at 22:56Hi   Im just wondering what are all the Pros and Cons of using CubeMX. Im really just starting to develop for the ST32 and have the free Keil suite and been using the CubeMX. Obviously one Pro is getting a project up...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.