2018-06-08 2:20 AM
Hi,
I have a problem to achieve max. sampling rate of 2.4 MSPS(12 Bit) @168 Mhz Clock, AHB2 Bus is running at 84 MHz and ADC Clock = 42 MHz.
Any idea why I get just sampling rate of 1.4 MSPS and not maximum sampling rate?
static void MX_ADC1_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = DISABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.NbrOfDiscConversion = 0; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING; hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO; // hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; sConfig.Offset = 0; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
I would be very thankful…
Cheers,
Ermin
2018-06-08 4:44 AM
Any idea why I get just sampling rate of 1.4 MSPS and not maximum sampling rate?
How do you know those 1.4MSPS?
JW
2018-06-08 6:53 AM
I sampled 100 kHz Sinus and got 14 values over one period. I just counted from lowest to lowest value among sampled values in Debugger.
E.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.