2021-05-06 2:02 PM
The IRQ is setup as follow:
__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
/*Configure the SysTick to have interrupt in 1ms time basis*/
HAL_SYSTICK_Config(SystemCoreClock/1000U);
/*Configure the SysTick IRQ priority */
HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority ,0U);
/* Return function status */
return HAL_OK;
}
But for some reason, it never gets triggered. TickPriority = 3
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.