2026-02-08 11:35 AM - edited 2026-02-08 11:51 AM
Hi,
I am using the application core of the STM32WB55VGY6 (not the radio core). I created a CubeMX project and added a simple HAL_GPIO_TogglePin() call. Literally just 2 lines of code in the entire project.
When I use a for loop as a delay, the code works as expected. However, when I use HAL_Delay(), it does not.
For some reason the SysTick_Handler() is never called...
I’ve attached the full project, including the .ioc file. The application code itself is minimal (only two lines).
From the configuration:
The timebase source is set to SysTick
Interrupts are enabled
The SysTick_Handler() is generated, but it is never triggered
Has anyone encountered this on the STM32WB application core, or have any suggestions on what might be missing or misconfigured?
Thanks.
Solved! Go to Solution.
2026-02-08 5:30 PM
Solved.
For those who might need this, for some reason on this part CubeMX sets the Systick priority to15 instead of 0.
Now it works.
2026-02-08 5:30 PM
Solved.
For those who might need this, for some reason on this part CubeMX sets the Systick priority to15 instead of 0.
Now it works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.