2012-04-24 12:13 AM
Hello everybody,
I have some troubel to communicate with m24LR64. I use a STM32L- Discovery. I try to see something in the oscilloscope but nothing, could you help me to see what is wrong in my code: #define I2C2_SLAVE_ADDRESS7 0xA0 // EEPROM I2C Address #define ClockSpeed 200000 // 200 KHz #include ''mainsee.h'' void I2Cmain(void) { GPIO_InitTypeDef GPIO_InitStructure; I2C_InitTypeDef I2C_InitStructure; /* I2C1 and I2C2 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE); /* GPIOB Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); /* Configure I2C2 pins: SCL and SDA ----------------------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_Pin_10, GPIO_AF_I2C2); GPIO_PinAFConfig(GPIOB, GPIO_Pin_11, GPIO_AF_I2C2); //I2C_DeInit(I2C2); /* I2C2 configuration ------------------------------------------------------*/ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = I2C2_SLAVE_ADDRESS7; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = ClockSpeed; I2C_Init(I2C2, &I2C_InitStructure); /* Enable I2C2 -------------------------------------------------------------*/ I2C_Cmd(I2C2, ENABLE); /* Send I2C1 START condition */ I2C_GenerateSTART(I2C2, ENABLE); /* Test on I2C1 EV5 and clear it */ // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM slave Address for write */ //I2C_Send7bitAddress(I2C2, I2C2_SLAVE_ADDRESS7, I2C_Direction_Transmitter); } /* Test on I2C1 EV6 and clear it */ // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); while(1){ /* Send I2C1 EEPROM internal address */ I2C_SendData(I2C2, 0x00); } /* Test on I2C1 EV8 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send I2C1 EEPROM data */ I2C_SendData(I2C2, 0x05); /* Test on I2C1 EV8 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send I2C1 STOP Condition */ I2C_GenerateSTOP(I2C2, ENABLE); while(1); // Do not exit } Thank you very much in advance to help me. P.S: Sorry for the english, i'm French.2015-01-07 12:31 AM
Hello Siddharth,
This is an old thread. Please try to describe your problem in a separate discussion giving more details on your case. This will be easier to provide you help.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.