2026-01-15 3:26 AM - last edited on 2026-01-16 7:00 AM by Andrew Neil
Hello there,
I'm trying to create a project for stm32h7s7 with external loader. But when i added the external loader in IOC file the all indexes were lost in editor mode. But I checked for building, i can't see any problem. I tried index -> rebuild but it could not help me
Solved! Go to Solution.
2026-01-21 2:10 AM
Hello @neset ,
Thank you for sharing your project.
I'm not able to reproduce the issue with STM32CubeMX 6.16.0 , STM32CubeIDE 2.0.0 and STM32Cube FW_H7RS V1.3.0 Cube firmware .
Could you please update your toolchains and the STM32CubeH7RS firmware versions and let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-16 5:20 AM
Hello @neset and welcome to the community;
Could you please share the ioc file?
Did you encounter a build error?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 1:26 AM
2026-01-21 2:10 AM
Hello @neset ,
Thank you for sharing your project.
I'm not able to reproduce the issue with STM32CubeMX 6.16.0 , STM32CubeIDE 2.0.0 and STM32Cube FW_H7RS V1.3.0 Cube firmware .
Could you please update your toolchains and the STM32CubeH7RS firmware versions and let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 4:35 AM
I'm using the STM32CubeIDE 1.17.0 (on Linux) perhaps the version couldn't support it. I will install the latest version and i ll give a result to you.
2026-01-27 1:10 AM
Hello @neset ;
Any update about this issue?
I used STM32CubeMX 6.16.0 and STM32CubeIDE 2.0.0 (on windows) for test.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-27 6:05 AM
Actually i installed the latest version of the CubeIDE and the issue fixed. But the ioc files cant editable in the IDE hence i dont like the new version of the IDE.
2026-01-27 11:41 PM - edited 2026-01-27 11:44 PM
Hello @neset ;
Glad to know that the issue is solved.
Thank you for sharing your feedback about the new STM32CubeIDE version. Y
Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. Please look at "STM32CubeIDE 2.0 release - early heads-up!" post.
STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the same way as with IAR EWARM, Keil MDK-ARM, and STM32Cube for VS Code.
I recommend you to create a new post in STM32CubeIDE forum and share your feedback.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.