2024-11-29 5:03 PM
Hi,
Has anyone used the STM32H750B-DK on-board eMMC, 4GB memory.
I have been unable to find an example and it is a big job to write something from scratch.
I am assuming that it would use the SDMMC1 peripheral in MMC 8 Bit mode and that you would need to port fatFs to it.
I cannot find any detailed data sheet on the THGBMTG5D1LBAIL / THGBMDG5D1LBAIL chips to get the correct timing data etc. Does anyone know where to get a detailed sheet. All that is readily available is a data brief for promotional purposes.
The parameter settings for the interface are pretty basic:
So it shouldn't be too difficult, but any help would be appreciated.
Kind Regards
Rob
Solved! Go to Solution.
2024-11-29 5:15 PM - edited 2024-11-29 5:17 PM
Doesn't the eMMC spec drive the timing expectations? Or impart via the EXTCSD
52 MHz should be sustainable, in a 1,4 or 8-bit SDR sense
Perhaps look at
STM32Cube_FW_H7_V1.9.1\Projects\STM32H745I-DISCO\Applications\FatFs\FatFs_Shared_Device
STM32Cube_FW_H7_V1.9.1\Drivers\BSP\STM32H750B-DK\stm32h750b_discovery_mmc.c
Been an age since I poked at this one.
Might be a bsp, display or demo one for the H750B
2024-11-29 5:15 PM - edited 2024-11-29 5:17 PM
Doesn't the eMMC spec drive the timing expectations? Or impart via the EXTCSD
52 MHz should be sustainable, in a 1,4 or 8-bit SDR sense
Perhaps look at
STM32Cube_FW_H7_V1.9.1\Projects\STM32H745I-DISCO\Applications\FatFs\FatFs_Shared_Device
STM32Cube_FW_H7_V1.9.1\Drivers\BSP\STM32H750B-DK\stm32h750b_discovery_mmc.c
Been an age since I poked at this one.
Might be a bsp, display or demo one for the H750B
2024-12-05 7:01 PM
Thanks for that I will have a look.
2025-06-03 9:14 PM
Is there any register we have to shift in order to access stm32h750b-dk's eMMC? I want to do file read , write file operations in eMMC but i am not able to do it. need help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.