2024-07-17 1:23 AM
I'm encountering an issue with the ADC on my STM32H745ZIT6 microcontroller when reading voltages from a power supply. Here's the problem in detail:
I'm using the ADC to convert analog voltages from a power supply into digital values. However, I've noticed significant inaccuracies in the ADC readings across all voltage ranges. For example, when the power supply outputs 6V, the ADC reads 6.22V consistently, and similar deviations occur across other voltage levels.
I've ensured that the power supply voltages are stable and within the operating range specified for the ADC. The issue is persistent and does not seem to be related to specific voltage thresholds.
Has anyone else in the community encountered similar issues with the STM32H7 series ADC? If so, how did you resolve them? Any insights or suggestions on how to troubleshoot or resolve this issue would be greatly appreciated.
2024-07-31 4:31 AM
TDK, thank you for the info, I've managed to set it manually as in the following flow:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.