2025-08-22 1:30 AM
I believe the STM32H743XGH6 has 1 MB of internal flash memory. However, using STM32CubeProgrammer, I was able to write and read data to the reserved area at 0x8180 0000. Is it okay to use this area?
The built-in Flash Memory areas of the STM32H743XGH6 are recognized as
0x8100 0000-0x817F FFFF and 0x8000 0000-0x0801 FFFF.
Solved! Go to Solution.
2025-08-22 2:08 AM - edited 2025-08-22 2:08 AM
Hello,
This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is NOT recommended.
2025-08-22 2:08 AM - edited 2025-08-22 2:08 AM
Hello,
This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is NOT recommended.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.