2025-05-29 2:11 AM - last edited on 2025-05-29 2:23 AM by Andrew Neil
We are currently using the STM32H723VGT6 MCU (1MB Flash) in our application.
We would like to clarify whether this MCU supports execute-in-place (XIP) from Quad-SPI flash or if Octal-SPI is required for XIP functionality.
In the future, if our application requires 2MB of internal flash, we plan to upgrade to the STM32H743VGT6, which is pin-to-pin compatible and also supports Quad-SPI.
As we are designing a common schematic for both MCUs, we would like to confirm:
Is a single Quad-SPI interface sufficient for enabling XIP on the STM32H723VGT6, or does it require an Octal-SPI interface for that purpose?
2025-05-29 2:47 AM
2025-05-29 3:31 AM
If the memory can be mapped it can be run. So yes this would work.
QUADSPI device are viable.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.