2023-12-30 7:43 PM - last edited on 2025-03-21 5:23 AM by Amel NASRI
I have had a couple of Nucleo 144 test/demo boards for a couple of years and have had no issues with them.
So I decided to try and create the simplest PCB from scratch.
What is happening is the chip itself is resetting when powered with a repeated signal as measured on an oscilliscope.
The devices is powered from a 3.6V LDO regulator that can provide 500mA.
Before I try to program the device I am trying to get the supply to the chip stable.
What I have done on connections all VDD and VSS connected with 100nF caps with the 4.7uF as specified.
I have POR-ON, NRST and BOOT0 pulled high through 10K resistors.
Now the USB (I am not using) VDD33USB I have connected to 3.6V which it says I can in the spec sheet and bypassed with a 100nF capacitor.
I have also connected and bypassed the VDDA pin also.
Am I missing something I need to do or does the empty chip reset itself this way until it is programmed?
Any suggestions would be greatly appreciated.
I have not exceeded the voltage limits.
2023-12-30 8:01 PM
A fresh chip will not reset itself--something is wrong.
Are VCAP pins connected and bypassed to GND with a 2.2 uF? Perhaps show the schematic.
> STM32H723GT6
This is missing a letter. STM32H723ZGT6 perhaps?
Design guide here:
2023-12-31 7:33 AM - edited 2023-12-31 7:35 AM
Thank you ... the real answer for me to progress further is the chip should not be visibly resetting.
Yes I do have 2.2uF caps bypass to ground on each VCAP.
Yes I missed the letter off the chip model.
So I am now considering the chip I have used as the 3.6V LDO is a production part I use on another device so well understood. The chip is of uncertain origin as it was obtained from a dubious source when supply was an issue.
I have 2 more though that I got from a reputable outlet so will assemble another for comparison.
So I consider my question answered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.