2019-04-11 8:34 AM
RM0433 Rev 5 writes:
The recommended single write sequence in bank 1/2 is the following:
1. Unlock the FLASH_CR1/2 register, as described in Section 3.5.1: FLASH configuration
protection (only if register is not already unlocked).
2. Enable write operations by setting the PG1/2 bit in the FLASH_CR1/2 register.
3. Check the protection of the targeted memory area.
4. Write one Flash-word corresponding to 32-byte data starting at a 32-byte aligned
address.
5. Check that QW1 (respectively QW2) has been raised and wait until it is reset to 0.
An5312 Rev 1 writes:
The recommended write sequence is updated as follows:
1. unlock the FLASH_CR1/2 register (only if register is not already unlocked)
2. enable write operations by setting the PG1/2 bits in the FLASH_CR1/2 registers
3. check the protection of the targeted memory areas
4. write one Flash memory word (corresponding to 32-byte) data starting at a 32-byte
aligned address
5. check that QW1/QW2 (respectively for FLASH_CR1/2) has been set high and wait until
it is reset to 0.
I have read multiple times and beside wording, where is the difference?
2019-04-12 4:03 AM
Hello,
In fact, the change was anticipated and implemented in the RM.
Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.