2019-04-12 2:25 AM
Hey guys
I'm currently wondering why i'm not reveiving any interrupts at all on my STM32F413
I used cube mx to create a new project.
For starters I'd like to send some data via UART with an interupt transfer.
uint8_t dummy[4] = { 0 };
volatile HAL_StatusTypeDef hal_uart_transmit = HAL_UART_Transmit_IT(&huart1, dummy, 4);
HAL_Delay(5000);I'm only transfering 4 byte. That should be possible within 5 Seconds =)
the hal_uart_transmit status tells me OK. But this does not say anything about the actual transfer status since it is an interrupt transfer.
My Expectation: I'd expect some sort of UART1 interrupt (doens't matter if TX complete, RXNE or error at the moment).
Therefore i set a breakpoint in the UART 1 IRQ Handler BEFORE calling HAL_UART_IRQHandler(&huart1);
But i'm never getting there. So there is something wrong with my interrupts.
I verified that MX_USART1_UART_Init() is called at the beginning of main()
void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_9B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_EVEN;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
}MX_UART1_Init calls the MSP Init which looks like this
void HAL_UART_MspInit(UART_HandleTypeDef* uartHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(uartHandle->Instance==USART1)
{
/* USER CODE BEGIN USART1_MspInit 0 */
/* USER CODE END USART1_MspInit 0 */
/* USART1 clock enable */
__HAL_RCC_USART1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**USART1 GPIO Configuration
PA9 ------> USART1_TX
PA10 ------> USART1_RX
*/
GPIO_InitStruct.Pin = UCE_USART1_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
HAL_GPIO_Init(UCE_USART1_TX_GPIO_Port, &GPIO_InitStruct);
GPIO_InitStruct.Pin = UCE_USART1_RX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
HAL_GPIO_Init(UCE_USART1_RX_GPIO_Port, &GPIO_InitStruct);
/* USART1 interrupt Init */
HAL_NVIC_SetPriority(USART1_IRQn, 7, 0);
HAL_NVIC_EnableIRQ(USART1_IRQn);
/* USER CODE BEGIN USART1_MspInit 1 */
/* USER CODE END USART1_MspInit 1 */
}
}So the UART Interrupt should be enabled.
Do you have any ideas, why the interrupts are not comming through?
My UART Tests runs as a first step, before anything else runs. Nobody could disable my UART interrupt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.