2019-12-07 9:12 PM
Hi
I made the processor STM32G030C6t6 , STM32G030K6t6 because it will be
cheap in the future and have a lot of use for it.
I use the Flash Loder Dmonstrator program for the STM32 processor program.
Due to the high number of daily programs and I have my own automatic programmer working with port COM.
The program identifies Flash Loder (v2.8) find processors but does not
have program addresses and does not work.
Please prepare a new edit to fix this issue.
Thanks
2020-03-13 11:58 PM
Hi@Samira
I had previously created a programmer that could program many processors at the same time as a serial port and I can program them repeatedly.
But with a problem with the new G030 series, rewriting must be programmed option byte (nboo0)to zero by another port !!!
These are weird forms and I don't know why they didn't think of them.
This problem can no longer be easily programmed with the serial port.
This problem reminds me of years ago when I used the AVR family. One Registry had an oscillator control input frequency to the processor
if you had an external crystal and this register on the input oscillator would no longer pass through the data processor.
The working month changed the value of the registry automatically, and we hardly attached an external oscillator and then programmed that registry.
Then you could re-program it.
I hope ST company does something about this problem.
Good luck.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.