2026-04-24 4:38 AM
I would like to use some of your
The problem is that i don't understand how to use your memory loader with these chips
The problem is that this library expects the chips to have 4 byte address and just doesn't work with 3 address chips. If you go through and just change all the call's to 3 byte address in the library i can make a STLDR file to talk to the chip. Just trying to see if there's a better way.
You have this custom memory section that would help i just don't know how to use it? So i'm hoping for some help there.
2026-04-24 8:14 AM
Hello @Brenden_PLUS
The better way is not to change the whole loader from 4-byte to 3-byte addressing everywhere. Instead, keep stm32-mw-extmem-ldr as the loader framework and create a small device-specific low-level driver for your EEPROM where the address length = 3 bytes is handled in one place.
2026-04-24 8:23 AM
I'm not sure what your suggesting.
I want to use the "stm32-mw-extmem-ldr as the loader framework". The problem is that it just can't do 4 byte address. For my program i have support for the chip, since i'm using zephyr.
The problem is i don't have a way to program the board. ST programmer using STLDR files and the sudgested program to use to make the STLDR for the N6 and H7 is stm32-mw-extmem-ldr. It works good just not for the smaller parts. There are custom parts in the repo. I just don't know how they are used. In that custom directory they have parts that start off with 3 byte address. I just don't know how to enable it.
2026-04-27 3:01 AM
Hello @Brenden_PLUS ,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.