2023-02-10 12:44 AM
Hi Community!
For a new project I need both external RAM and external
FLASH memory (from which code should also be executed) on a
STM32F767BG.
Now I'm faced with the question of what makes more sense:
• SRAM on FMC and Flash on QPSI
• Or SRAM and Flash both on the same FMC
Can you say in general what is more efficient and performant with regard to
Waiting and access times? Can you also say in general whether NOR or NAND
Flash is preferable?
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.