2023-02-09 8:40 AM
2023-02-10 1:38 AM
This the STM32F469. I resolved the problem. This is the latency of FLASH_ACR who is at 3 for the HCLK at 100MHz
Thanks
2023-02-09 8:47 AM
> STM32F486
There is no such.
> it doesn’t work anymore
What does it mean?
JW
2023-02-09 9:57 AM
The STM32L486 ? That's only rated to 80 MHz operation
https://www.st.com/en/microcontrollers-microprocessors/stm32l486rg.html
It might get to 100 MHz, but if it is failing it either needs more wait states on the flash, or you've tickled a critical path.
2023-02-09 11:32 PM
Sorry, I use the STM32L469
2023-02-10 12:24 AM
> Sorry, I use the STM32L469
There is no such, either.
> it doesn’t work anymore
What does it mean?
JW
2023-02-10 1:38 AM
This the STM32F469. I resolved the problem. This is the latency of FLASH_ACR who is at 3 for the HCLK at 100MHz
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.