2016-05-03 5:08 AM
Hi,
any idea when support for these is out? I've got a 767ZI... I whacked on a nucleo board and would like to check out some DP FPU stats,regards2016-05-10 2:13 PM
Attached is a small Nucleo-144 F7 test app, outputs via the VCP USART at 115200 8N1
________________ Attachments : gnu_f767zi_nucleo_demo_rel1.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0hM&d=%2Fa%2F0X0000000bcd%2FzuCHvwPEE0dh8OlWznZZrzIcH..EDgHhd43aoeYdnp8&asPdf=false2016-05-23 1:24 PM
Ok, so any update about when in ''May'' this and the Reference Manual might appear?
Can someone light a fire under sales/marketing?2016-05-27 5:37 AM
CMSIS and new F7 examples can be found within
http://www.keil.com/pack/Keil.STM32F7xx_DFP.2.6.0.pack
a .ZIP file2016-05-27 6:44 AM
Hi clive1,
New STM32F7 devices arehttp://www.st.com/content/st_com/en/about/media-center/press-item.html/n3822.html
to be in mass production yesterday.Various examples are provided within the new boards dedicated directories in the new package version (1.4.0).The reference manual of STM32F76x and STM32F77x devices is .All your feedback are welcome. This will help us to improve our offer.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-05-27 3:52 PM
Conveniently the Nucleo-F767ZI arrived today. The attached example built in GNU/GCC from earlier in the month runs as hoped...
Testing printf
STM32 2048 KB FLASH, 512 KB RAM, 0046002F-33355109-36343130 UNIQUE
C0000000 FFFFFFF8 00000000
10110221 12000011 00000040
FPU-D Single-precision and Double-precision
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.